CharBufferString.Init (METH)

METHOD Init : BOOL

Init method used for using an already existing memory for storing the string

InOut:

Scope

Name

Type

Comment

Return

Init

BOOL

Input

pBuffer

POINTER TO BYTE

The pointer to the buffer containing the string

uiBufferSize

UINT

The size of the buffer (in bytes), where the string is stored. If this value is 0, no memory is allocated and the CharBufferPtr pointer has to be set by calling the Initialize method

stringType

__SYSTEM.TYPE_CLASS

A __SYSTEM.TYPE_CLASS value indicating type of the string