StrCaseCmpEndA (FUN)

FUNCTION StrCaseCmpEndA : INT

Does a case insensitive comparison of the end of the string and the suffix

Return values:

0 -> end of the string and suffix are equal

-1 -> end OF the STRING AND suffix are NOT equal

-2 -> Error: An invalid string (ie. Null-Pointer is given)

InOut:

Scope

Name

Type

Comment

Return

StrCaseCmpEndA

INT

Input

pString

CharBufferPtr

Pointer to the string to check.

pSuffix

CharBufferPtr

Pointer to the suffix to find.