FUNCTION StrCmpEndA : INT
Does a case sensitive comparison of the end of the string and the suffix
Return values:
0 -> end of the string and suffix are equal
-1 -> end of the string and suffix are NOT equal
-2 -> Error: An invalid string (ie. Null-Pointer is given)
InOut: |
|