INTERFACE IPaintAfterAllRectangleProvider EXTENDS IPaintAfterAll
This interface is the equivalent to IRectangleProvider which will be called for paint after all elements when these are open. The interface can be implemented optionally too by functionbloxk implementing IPaintAfterAll
Methods:
PAAClose, inherited from IPaintAfterAll
PAAgetSize, inherited from IPaintAfterAll
PAAgetSurroundingRect, inherited from IPaintAfterAll
PAAgetUpdateRects, inherited from IPaintAfterAll
PAAhandleInputBefore, inherited from IPaintAfterAll
PAApaintAfterAll, inherited from IPaintAfterAll
Structure: