VisuFbClientTagDataHelper (FB)

FUNCTION_BLOCK VisuFbClientTagDataHelper

This functionblock can be used to access the client tag data optionally contained in a visualization client object. As compiling this function block requires a device of version 3.5.5 at least, instances should be created only when such a device is used.

InOut:

Scope

Name

Type

Comment

Input

pClientData

POINTER TO VisuStructClientData

A pointer to a clientstructure to evaluate the according information from.

Output

xError

BOOL

An error was encountered

xIPv4Valid

BOOL

The client structure contains a valid IPv4 information within stIPv4

stIPv4

STRING

The IPv4 information; valid only if xIPv4Valid yields true

xNameValid

BOOL

The client structure contains a valid name information within stName

stName

STRING

The name information; valid only if xNameValid yields true

xRTVTargetIdValid

BOOL

The client structure contains a valid targetidentification of the Remote Targetvisualization. Only relevant for clients of that type.

dwRTVTagetId

DWORD

The targetidentification of the Remote Targetvisualization. Only valid if xRTVTargetIdValid yields true Only relevant for clients of that type.

xRTVTargetVersionValid

BOOL

The client structure contains a valid targetversion of the Remote Targetvisualization. Only relevant for clients of that type.

RTVTargetVersion

VERSION

The targetversion of the Remote Targetvisualization. Only valid if xRTVTargetIdValid yields true Only relevant for clients of that type.