VisuFctPaintSelection (FUN)

FUNCTION VisuFctPaintSelection : BOOL

Executes the drawing commands that are needed to draw the current element selection

InOut:

Scope

Name

Type

Comment

Return

VisuFctPaintSelection

BOOL

Input

pCurrentSelectionData

POINTER TO Visu_StructSelectionData

The current selection data

selectionColors

VisuStructColors

The current selection colors

selectionLook

VisuStructElementLook

The current selection look

iFrameOffset

INT

The offset of the selection frame

iPositionIndex

INT

The current position in the position array

dwPaintFlags

DWORD

Additional paint flags

iRadius

INT

elementType

VisuEnumSimpleType

pElementTexts

POINTER TO VisuStructElementTexts

optional element texts

pElementTextProperties

POINTER TO VisuStructTextProperties

optional element texts properties

pTextChanges

POINTER TO VisuFbAnalyzeTextVars

optional element text variables

pClientData

POINTER TO VisuStructClientData

Inout

elementPosition

VisuStructPaintRectangle

elementState

VisuStructElementState