|
Input
|
udiAlarmID
|
UDINT
|
|
The internal IDs of the alarm, the alarm class and the alarm group
|
|
udiAlarmClassID
|
UDINT
|
|
|
|
udiAlarmGroupID
|
UDINT
|
|
|
|
liTimestapLast
|
TIMESTAMP
|
|
The several timestamps of the alarm
|
|
liTimestapActive
|
TIMESTAMP
|
|
|
|
liTimestapInactive
|
TIMESTAMP
|
|
|
|
liTimestapAcknowledge
|
TIMESTAMP
|
|
|
|
iOffsetLast
|
INT
|
-1
|
The several offsets of the alarm
|
|
iOffsetActive
|
INT
|
-1
|
|
|
iOffsetInactive
|
INT
|
-1
|
|
|
iOffsetAcknowledge
|
INT
|
-1
|
|
|
usiPriority
|
USINT
|
|
The priority of the alarm class the alarm belongs to
|
|
eState
|
AlarmState
|
|
The current state of the alarm
|
|
ePrevState
|
AlarmState
|
|
The previous state of the alarm
|
|
byTriggerValueType
|
BYTE
|
|
The several values attached to the alarm. For each value we store the type class value as BYTE and an 8 byte value representing the value.
|
|
liTriggerValueVal
|
LINT
|
|
|
|
pLatchVariables
|
POINTER TO ARRAY [0..10] OF LatchVariable
|
|
Will be set by the code generation and contains the memory, where the latch variables can be stored (the size 0..10 is only for debug reasons)
|
|
usiCountLatchVariables
|
USINT
|
|
|
|
itfAlarm
|
IAlarm
|
|
The IAlarm instance, where the data of this structure comes from
|
|
idRow
|
CAA.IDENT
|
|
The row ID of the alarm in the alarm storage, or the original row id for remote alarm
|
|
xIdRowValid
|
BOOL
|
|
|
|
sRemoteDeviceName
|
STRING
|
|
If the above row id is valid, used only in distributed alarm handling The name of the remote device in case of remote alarm
|