FUNCTION ElaborateLatchFilterCriteria : BOOL
This method is an helper for the customer It elaborates the criteria for the filtering by latch 1 variable and send back the parameters to use
InOut:
|
Scope
|
Name
|
Type
|
Comment
|
Return
|
ElaborateLatchFilterCriteria
|
BOOL
|
|
Input
|
filterType
|
EFilterLatchContent
|
Filter type to use
|
filterValue
|
WSTRING
|
Filter value
|
Output
|
filterTypeElab
|
EFilterLatchContent
|
Filter criteria after the elaboration
|
wsValue
|
WSTRING
|
Filter value in case of filter criteria is “STRING”
|
vType
|
Visu_Types
|
Type of the elaborated value
|
liValue
|
LINT
|
Numerical value elaborated
|
rValue
|
REAL
|
Numerical value elaborated in case of REAL
|
lrValue
|
LREAL
|
Numerical value elaborated in case of LREAL
|
|