METHOD Execute
Executes the action.
Scope
Name
Type
Comment
Input
eCurrTransition
AlarmStateTransition
The currently processed alarm state transition. This will be evaluated in order to determine, whether the action has to be executed or not
itfAlarm
IAlarm
The alarm, for which the action has to be performed
pbyAdditionalData
POINTER TO BYTE
An optional pointer to a structure variable containing additional parameter