CAA Technical Workgroup
CAA Real Time Clock Extern
3.5.17.0
Intern|CAA|System
RTCLK
3S - Smart Software Solutions GmbH
CAA RTCLK
Vendor specific library for real time clock access.
CAA Real Time Clock
Enums
Function Blocks
Functions
GlobalConstants
Structs
GetSupplierVersion (Function)
VersionConstants (GVL)
[1]
Based on CAA Real Time Clock Extern.library, last modified 20.04.2021, 14:34:06. LibDoc 4.0.0.0
The content file CAA Real Time Clock Extern.clean.json was generated with CODESYS V3.5 SP16 Patch 3 on 20.04.2021, 14:34:06.