The tab shows the object directory of the ESI file or the slave.
Requirement: The application is in online mode. The expert settings in the Slave dialog have to be enabled and the slave has to support CoE.
Read objects |
The object directory is read one time. |
Auto update |
The objects are read in cycles. |
Offline from ESI file |
The dialog shows the contents of the object directory from the device description. |
Online from device |
The dialog shows the contents of the object directory of the device. |
Flags |
|
Type |
Data type of the parameter |
Value |
You can double-click in the text field to edit this value. |