Tab: EtherCAT Slave – EoE Settings

This tab is used to configure the communication settings for the individual slaves that support Ethernet over EtherCAT (EoE).

Requirement:

Settings

Virtual Ethernet Port

: Enables the EOE functionality of the slave. A unique Virtual MAC ID has to be defined.

Virtual MAC ID

Input field for the Virtual MAC ID

Switch port

: The device acts as a switch. No additional network settings are required.

IP port

: The device acts as an IP port. The IP Settings have to be configured.

IP Settings

The Ethernet communication parameters have to be set according to the parameters of the virtual Ethernet adapter.

IP address

IP address of the slave in the network (length: 4 bytes)

The IP port has to be in the same range as the virtual Ethernet adapter. For example, if the address of the network adapter is 192.168.1.1 and the subnet mask is 255.255.255.0, then the IP port has to be in the range from 192.168.1.2 to 192.168.1.254.

Subnet mask

Subnet mask (length: 4 bytes)

Default gateway

Default gateway (length: 4 bytes)

DNS server

IP address of the DNS server

DNS name

Name of the DNS server