CODESYS Scripting allows you to automate commands or complex program operations in CODESYS, which otherwise require manual mouse clicks and text input in the CODESYS user interface. For this purpose, scripts based on (Iron)Python can be started from the CODESYS user interface (command or configured toolbar) or from the Windows command line.