With the CODESYS Visualization add-on, within your project you can create the suitable user interface for your application. In order to visualize this, you link a visualization to your application data.
When creating a visualization and an application, you have the advantage that you can use common functions, for example, as library and source code management or find/replace throughout the project.
NOTICE | |
---|---|
For more information, see: "Best Practices, Visualization" document. It is provided as a PDF with the CODESYS installation.