Switch to legacy user management

NOTE:

Whenever possible, use a runtime version >= 3.5 SP18 Patch 1 and CODESYS Visualization version >= 4.2.0.0 for a new project with a visualization.

You have initially created a runtime-based user management. Now you want to decouple this from the device user management and have a separate management only for the visualization users.

  1. In the Visualization Manager, open the User Management tab and click the Groups tab.

  2. Click the Convert to Legacy button.

    • User management is decoupled from device user management and converted to legacy. The Users tab opens.