The Safe Direction safety-related function ensures that rotation/movement is only possible in the permitted (parameterized) direction.
The function block distinguishes two rotation/movement directions by providing separate inputs for requesting the SDI Negative or SDI Positive monitoring function: SDIneg and SDIpos. Both SDI monitoring functions are configured using the same parameters but can be requested independent of each other.
In which physical rotation/movement direction SDIpos or SDIneg actually results, depends on your application.
If SDIpos and SDIneg are requested at the same time, the SS1 function is automatically executed as the defined fallback function.
The SDIneg/SDIpos function prevents the motor from rotating more than a defined amount into the incorrect direction (device parameter SDI_PositionTolerance[sTol], see below).
The request of the safety-related function occurs at the beginning of the t1 time interval ('S_SDI*_Request' signal in the diagram). t1 is set with the device parameter SDI_StartDelayTime[t1].
Within the t1 time interval, the standard (non-safety-related) controller also receives the request from the connected process and initiates the motion control function according to the logic and drive parameterization defined in the standard (non-safety-related) application.
After t1 has elapsed, the direction is monitored by capturing the actual position. Moving/rotating a certain distance against the allowed direction is permitted if it does not exceed the defined position tolerance STol.
If the SDI function is executed successfully, the function block switches S_SDI*_SafetyActive = SAFETRUE (see diagram).
If the SS1 fallback function has been activated due to an error detected of the position tolerance as described below, this is indicated by S_SS1_SafetyActive = SAFETRUE.
If the actual position moves more than the set position tolerance (parameter SDI_PositionTolerance[sTol]) into the wrong direction, the SS1 function is automatically executed as the fallback function.
The SDI function is used to ensure that rotation or movement is not possible towards a prohibited direction, e.g., when personnel accesses the zone of operation of a machine.
To implement this safety function in your safety-related application proceed as follows:
In Machine Expert 'Devices' window, insert a safety module for the drive used.
In Machine Expert – Safety, insert a Preventa Motion FB SF_SafeMotionControl into the safety-related code and connect it accordingly.
In the Machine Expert – Safety 'Devices' window, mark the safety module in the devices tree and edit the safety-related parameters in the 'Mechanic' group and in the 'SafeDirection' group.
For details, refer to the parameter description of the Lexium 62 LXM Safety Option Module/Lexium 62 ILM Safety Option Module.