Overload Control

 

Overview

This part explains the functionality and implementation of the Overload control functions in the Hoisting Library.

What Is in This Part?

This part contains the following chapters:

oOverload Control Function: Detect Mechanical Overload on Hoisting Devices

oOverload_EN15011: Overload Calibration With the Requirements of EN15011