FB_RobotTSeries - GetDigitalTwinConfigData (Method)

Overview

Type:

Method

Available as of:

V2.14.0.0

Versions:

Current version

This chapter provides information on:

Task

Get the configuration data for the EcoStruxure Machine Expert Twin communication of the Lexium T Robot.

Description

By calling the method, the configuration data for the OPC UA data structure of the Lexium T Robot can be read.

Interface

Output

Data type

Description

q_etDiag

GD.ET_Diag

General, library-independent statement on the diagnostic.

A value not equal to ET_Diag.Ok corresponds to a diagnostic message.

q_etDiagExt

ET_DiagExt

POU-specific output for the diagnostic.

q_etDiag = ET_Diag.Ok -> Status message

q_etDiag <> ET_Diag.Ok -> Diagnostic message

q_sMsg

STRING[80]

Event-triggered message that gives additional information on the diagnostic state.

q_stData

DTC.ST_ConfigDataRobotTSeries

Read out the data that have been configured to emulate this robot in EcoStruxure Machine Expert Twin.

Diagnostic Messages

q_etDiag

q_etDiagExt

Enumeration value

Description

OK

OK

0

Successful

ExecutionAborted

RobotNotInitialized

89

The robot is not initialized.

ExecutionAborted

DigitalTwinConfigDataNotSet

128

Configuration data for EcoStruxure Machine Expert Twin has not been set.

RobotNotInitialized

Enumeration name:

RobotNotInitialized

Enumeration value:

89

Description:

The robot is not initialized.

Issue

Cause

Solution

Reading the EcoStruxure Machine Expert Twin configuration parameter was unsuccessful.

The robot is not initialized.

Verify that the robot has been initialized successfully.

DigitalTwinConfigDataNotSet

Enumeration name:

DigitalTwinConfigDataNotSet

Enumeration value:

128

Description:

Configuration data for EcoStruxure Machine Expert Twin has not been set.

Issue

Cause

Solution

Reading the EcoStruxure Machine Expert Twin configuration parameters was unsuccessful.

The EcoStruxure Machine Expert Twin configuration parameters have not been set

Verify that the method SetDigitalTwinConfigData has been called successfully.