IScriptConventionsObject

class

IScriptConventionsObject.

IScriptConventionsObject

Bases: object

Scripting API attached to conventions table objects.

conventions_table

contextNodeUri=None

Starts the Code Analysis and returns the conventions table for requested query chains.

Parameters

contextNodeUri (string) -- The context node uri of a folder in application tree, if only a specific part of the application should be analyzed. If not set, the whole application or POU area (in case of a library) is analyzed.

Returns

Conventions table result.