class
IScriptTestRun.
IScriptTestRun
Bases: object
Functionality for handling a test run.
init_values
Retrieves or sets the test run parameters. These values are used to initialize a test data type (DUT) with the values defined by the user for a test run.
List of string
user_comment
Retrieves or sets a user comment for the test run.
string
run_id
Identifies a test run in a test set.
uint