Output signal of the function block (enable signal).
Data type: SAFEBOOL
Following activation of the function block (with Activate = TRUE), the value of the output signal depends on the values at the function block inputs S_ChannelA and S_ChannelB, and also on whether or not the function block has detected an error.
As the enable signal is present at the S_EquivalentOut output, this output is also referred to as the enable output.
Connection: Connect this output to other safety-related function blocks/functions.
The function block supports a safety-related monitoring function but not a safety-related control function.
WARNING | |
---|---|
Permanent signals (S_ChannelA = SAFETRUE and S_ChannelB = SAFETRUE) at the inputs when the function block is activated (Activate = TRUE) or when the Safety Logic Controller is started up switch the enable signal (S_EquivalentOut) to SAFETRUE.
Value |
Description |
---|---|
SAFETRUE |
The S_EquivalentOut output can only be SAFETRUE if the following conditions are met:
|
SAFEFALSE |
The S_EquivalentOut output is SAFEFALSE if
|