Edge-triggered input for resetting error messages if the cause of the error is no longer present.
Data type: BOOL
Initial value: FALSE
The Reset input supports manual resetting of an active start-up or restart inhibit by the operator (see EN ISO 13849-1).
Resetting does not occur with a negative (falling) edge, as specified by standard EN ISO 13849-1, but with a positive (rising) edge.
Additional measures, e.g., an additional function stop, can be taken to reduce the risk of an unintended start-up.
Connection: With the signal of a reset button connected to the Safety Logic Controller (value TRUE or FALSE). Constant TRUE or FALSE values are not permitted.
Value |
Description |
---|---|
FALSE |
Error resetting and removal of an active start-up inhibit are not requested. |
Edge FALSE > TRUE |
Error resetting and removal of an active start-up inhibit are requested. The function block performs internal edge monitoring for the Reset input. A reset is only executed on a positive signal edge. A further static TRUE signal after a positive signal edge has no effect. |
Resetting the function block by means of a positive signal edge at the Reset input can cause the S_Mode0Sel..S_Mode7Sel output to switch to SAFETRUE immediately (depending on the status of the other inputs).
WARNING | |
---|---|
If the function block is expecting a positive edge for resetting (inhibit is active or an error state applies), a static TRUE signal at Reset will be regarded as an error. In such cases, switch Reset to FALSE to exit the error state.