Only you, the user, machine builder or system integrator can be aware of all the conditions and factors realized in the design of your application for the machine. Therefore, only you can determine the automation equipment and the related safeties and interlocks which can be properly used, and validate such usage.
WARNING | |
---|---|
The following conditions lead to an error message being produced at the function block (Error = TRUE and S_OSSD_Out = SAFEFALSE at the same time).
Exceeding the test time set at TestTime during the sensor test.
No response from the sensor during the sensor test.
Invalid static TRUE signals at Reset.
Invalid value for TestTime.
Plausibility errors are errors which occur, for example, when a range of values is exceeded or an impermissible connection is made. Such errors are detected and reported either by the function block itself or while the project is being compiled. However, this is not always possible in the case of connection errors.
This means that it is not possible, for example, to automatically verify whether:
Values or constants within the range of validity at inputs are, in fact, incorrect for the safety-related function executed.
This does not apply to a static TRUE signal at the Reset input. This is detected by the function block and reported as an error.
Inputs and/or outputs are incorrectly connected or are not connected when they should be.
WARNING | |
---|---|
If no additional exception avoidance measures are taken, signal levels which switch or toggle sporadically have the following effects:
At the edge-triggered inputs, such signals cause the function block to interpret the signal as an edge and trigger a potentially undesirable corresponding action.
At the state-controlled inputs, such signals cause the signal to trigger a potentially undesirable corresponding action.
Impermissible signals at inputs can lead to an unintended start-up, prevent a requested action from being executed or cause an error.
These signals may be caused by:
Programming errors in the application program (user errors).
Cross circuit, short circuit, and cable break (user errors, wiring errors).
To prevent this, the following measures can be taken, depending on the safety-related function:
Using safety-related device signals.
Using options for cross-circuit detection.
Verifying the safety-related code in the code editor followed by validation of all safety-related networks.
The measures listed above can also be taken in combination in order to help prevent cascading or otherwise difficult to detect errors.
If a start-up inhibit following activation of the function block is specified by the setting S_StartReset = SAFEFALSE, a static TRUE signal at the Reset input when the Safety Logic Controller starts up leads to a function block error message (Error = TRUE).
If the start-up inhibit is not in use when the Safety Logic Controller starts up (S_StartReset = SAFETRUE), the signal state at the Reset input is not relevant at this time. In such cases, the signal at the S_OSSD_Out output depends exclusively
on the status of the connected safety equipment
and on the setting at S_AutoReset (restart inhibit).
In order to reduce the risk of an unintended start-up, it is essential to ensure that the Reset input is only connected to the signal of a manual reset device. The risk analysis determines how this signal is to be set up in practice.
Inoperable or error producing safety equipment can only be detected by testing whether it is functioning correctly. The function block does not support function testing.
Possible causes of inoperable or error producing safety equipment are:
Inoperable devices (hardware errors)
Cross circuit, short circuit, and cable break (user errors, wiring errors)
WARNING | |
---|---|