IRectangleListManager.ForwardCallWithMouseDownInfo (METH)

METHOD ForwardCallWithMouseDownInfo

InOut:

Scope

Name

Type

Comment

Input

pElements

POINTER TO ARRAY [0..0] OF IVisualElement

count

INT

pMouseDownInfo

POINTER TO ARRAY [0..100] OF BYTE

a pointer to an array of bytes representing a bitfield with the information about elements handling mouse down or not the according bitfield is organized from lower indices to higher indices in general, within single bytes earlier elements are located at less significant bits