|
Input
|
itfVisuStreamReader
|
IVisuStreamReader
|
This must be an instance of IVisuStreamReader, that provides the data sent from the plc to the visualization
|
|
pxOptTransferActive
|
POINTER TO BOOL
|
Point to an optionally configured BOOL variable, that will indicate, whether currently the streaming is active
|
|
pxOptTransferSuccessful
|
POINTER TO BOOL
|
Point to an optionally configured BOOL variable, that will indicate, whether the last streaming was successful or not
|
|
pxOptErrorCode
|
POINTER TO Visu_AllNumericTypesUnion
|
Point to an optionally configured numeric variable, that will receive the error code
|
|
tcOptErrorCodeType
|
__SYSTEM.TYPE_CLASS
|
Contains the type of the variable pxOptErrorCode points to
|
|
xDoNotUsePropertyInfo
|
BOOL
|
This flag is TRUE, when called from the generated code of the visualization, where the compiler define VISU_USEPROPERTYINFO might be defined.
|
|
dwControlFlags
|
DWORD
|
|