IVisuUserEventManager.SetMouseEventHandler (METH)

METHOD SetMouseEventHandler : BOOL

This method assigns the eventhandler for mouse events. The method will return <c>TRUE</c> when there was no previous handler, and <c>FALSE</c> when there was a previous event handler.

InOut:

Scope

Name

Type

Return

SetMouseEventHandler

BOOL

Input

handler

IMouseEventHandler