METHOD SwitchToVisuByIndex : INT
It switches the visualization using the index instead of the frame path
|
InOut:
|
|
Scope
|
Name
|
Type
|
Comment
|
|
Return
|
SwitchToVisuByIndex
|
INT
|
|
|
Input
|
iIndexFrame
|
INT
|
The internal array index of the frame that should be handled
|
|
pClientData
|
POINTER TO VisuStructClientData
|
The client whose frame content shall be changed
|
|
iIndex
|
INT
|
The index of the visualization that should be selected
|
|
xUpdVar
|
BOOL
|
If also the variable linked to the frame has to be updated
|
|
xUpdLastIndex
|
BOOL
|
If also the index stored as “last call” has to be updated (specifically used in redundancy)
|
|