VisuFctTextAddOffset (FUN)

FUNCTION VisuFctTextAddOffset

It adds the offset to a recatngle used for text display (in DrawText…)

InOut:

Scope

Name

Type

Comment

Input

pTextPosition

POINTER TO VisuStructPaintRectangle

Actual rectangle, already rotated if the angle is present

textProperties

VisuStructTextProperties

Text properties, to get the alignemets

iOffsetH

INT

Horizontal offset, in pixel

iOffsetV

INT

Vertical offset, in pixel

iAngle

INT

Angle by which the rectangle is rotated

pCenter

POINTER TO VisuStructPoint

Center of rotation