Power Rails: Inserting

  1. Mark the object where you want to insert the power rail.

  2. Depending on the needed power rail type select either 'Objects > Power rail left' or 'Objects > Power rail right'.

The 'Power rail left/right' menu items are inactive if the corresponding power rail type cannot be connected to the selected object (e.g., directly to a formal parameter or a left power rail to a coil output).

NOTE:

It is not possible to insert a power rail which is not connected to any object.