EQ / EQ_S - Comparison: =

This comparison function compares the operands connected to the input parameters in regard to equality. Comparison proceeds from left to right. The function is available as standard function EQ and safety-related function EQ_S.

EQ

Parameter

Data types

Description

IN1

ELEMENTARY

First input value

IN2

ELEMENTARY

Second input value

OUT

BOOL

TRUE if the inputs are equal.

FALSE if the inputs are not equal.

EQ_S

Parameter

Data types

Description

IN1

SAFEELEMENTARY

First input value

IN2

SAFEELEMENTARY

Second input value

OUT

SAFEBOOL

TRUE if the inputs are equal.

FALSE if the inputs are not equal.

NOTE:

All input parameters must have the same data type.