Basic IEC 61131-3 Functions (safety-related and standard)

Functions are POUs with multiple input parameters and one output parameter. As they do not have any internal memory, a function called with the same input values always returns the same result. The abbreviation for functions is FU.

IEC 61131-3 describes basic functions. A subset of these functions are implemented in EcoStruxure Machine Expert - Safety.

NOTE:

Term definition: Standard = non-safety-related

The term "standard" always refers to non-safety-related items. Examples: a standard process data item is only read/written by a non-safety-related I/O device (i.e., a standard device). Standard variables/functions/FBs are non-safety-related data. The term "standard controller" designates the non-safety-related controller.

NOTE:

Standard functions are only allowed for programming standard program parts.

When programming a safety-related application a strict separation between safety-related and standard logic (networks) is required. Due to this, all IEC 61131-3-defined functions are also available as safety-related functions.

Representation

In the Edit Wizard the standard functions are represented by the symbol , in a code worksheet they appear in gray accordingly:

Safety-related functions are represented by the symbol in the Edit Wizard and appear in red when inserted in a code worksheet: