LE / LE_S - Comparison

This comparison function compares the operands connected to the input parameters in regard to less/equal. Comparison proceeds from left to right. The function is available as standard function LE and safety-related function LE_S.

NOTE:

The comparison is always a signed comparison. Therefore the values for DWORD are limited to 31 bits, for WORD to 15 bits and for BYTE to 7 bits.

LE

Parameter

Data types

Description

IN1

ELEMENTARY

First input value

IN2

ELEMENTARY

Second input value

OUT

BOOL

TRUE if IN1 is less or equal than IN2.

FALSE if IN1 is greater than IN2.

LE_S

Parameter

Data types

Description

IN1

SAFEELEMENTARY

First input value

IN2

SAFEELEMENTARY

Second input value

OUT

SAFEBOOL

TRUE if IN1 is less or equal than IN2.

FALSE if IN1 is greater than IN2.

NOTE:

All input parameters must have the same data type.