FUNCTION EncodeSpec : DWORD
This function servers to create the parameter dwSpec of type DWORD, which is necessary for callback functions, out of two values of type EVENT and EVENT_SOURCE.
Scope
Name
Type
Comment
Return
EncodeSpec
DWORD
Input
eEvent
EVENT
Event to be used
eClass
EVENT_CLASS
Event class to be used