NMT (FB)

FUNCTION_BLOCK NMT EXTENDS CiA405Base

This function block provides NMT services. The NMT request will be sent to the NodeID specified in input DEVICE. If NMT request should be addressed to all devices (including NMT master and sending device) set DEVICE to 0 . If all devices but not NMT master and sending device should be addressed use the additional flag TRANSITION_STATE.ALL_EXCEPT_NMT_AND_SENDER.

InOut:

Scope

Name

Type

Initial

Comment

Inherited from

Input

NETWORK

USINT

1

CAN network number the function block should operate on. Note: It is not the same like the network number in CANBus configurator. The CiA405 NETWORK is calculated by NetID + 1. Example: 1 = CAN0, 2 = CAN1, 3 = CAN2, …

CiA405Base

ENABLE

BOOL

FALSE

Enables the function block on rising edge. Aborts operation on falling edge.

CiA405Base

TIMEOUT

UDINT

0

Timeout in ms; 0 means no timeout

CiA405Base

Output

CONFIRM

BOOL

FALSE

TRUE: function block finished without error

CiA405Base

ERROR

CANOPEN_KERNEL_ERROR

CANOPEN_KERNEL_ERROR.CANOPEN_KERNEL_NO_ERROR

Error code: see CANOPEN_KERNEL_ERROR for further details

CiA405Base

Input

DEVICE

DEVICE

0

NodeID of destination device (local or remote). 0 means all devices.

STATE

TRANSITION_STATE

0

The NMT transition which should be performed.