TYPE DEVICE_STATE :
This enumeration lists all possible states of a device. The mapping to the according fieldbus specific states is defined by the associated fieldbus stack.
Attributes:
|
|
InOut:
|
Name
|
Comment
|
UNKNOWN
|
The device state is unknown.
Example: No supervision mechanism active.
|
STOPPED
|
The device is stopped.
|
RUNNING
|
The device is running.
|
ERROR
|
The device is in error state.
GetDeviceError may supply a specific error code.
|
DISABLED
|
The device is disabled in device tree.
|
NOT_CONFIGURED
|
The device has not yet been configured by the stack.
Example: Configuration phase not started yet.
|
CONFIGURED
|
The device has been configured by the stack.
Example: Configuration phase finished but device is not in running state.
|
NOT_FOUND
|
The device was not found on bus.
|
|