IBus.GetBusDiagnosisInfo (METH)

METHOD GetBusDiagnosisInfo : ERROR

Returns a DiagnosisInfo if xDiagnosisInfoAvailable of IBus.GetBusState was true.

Note

The interpretation of pData is fieldbus dependent and will be specified by the associated fieldbus driver.

InOut:

Scope

Name

Type

Comment

Return

GetBusDiagnosisInfo

ERROR

Input

pData

CAA.PVOID

Pointer to memory

szSize

CAA.SIZE

Size of memory in bytes where pData is pointing to

Output

szCount

CAA.SIZE

Number of Bytes written to pData