Input
|
xExecute
|
BOOL
|
Rising edge: Action starts
Falling edge: Resets outputs
If a falling edge occurs before the function block has completed its action, the outputs operate in the usual manner and are only reset if either the action is completed or in the event of an error. In this case, the corresponding output values (xDone, xError) are present at the outputs for exactly one cycle.
|
ETrig
|
Output
|
xDone
|
BOOL
|
TRUE: Action successfully completed
|
ETrig
|
xBusy
|
BOOL
|
TRUE: Function block active
|
ETrig
|
xError
|
BOOL
|
TRUE: Error occurred, function block aborts action
FALSE: No error
|
ETrig
|
Input
|
sFileName
|
CAA.FILENAME
|
File name, absolute or relative path specification
|
|
eFileMode
|
MODE
|
File mode: FILE_MWRITE - write, FILE_MREAD - read, FILE_MRDWR - read & write, FILE_MAPPD - append
|
|
xExclusive
|
BOOL
|
UNSUPPORTED PARAMETER: IS ALWAYS FALSE!
|
Note: Because of the POSIX behaviour of the file open functions on targets, there is no way to support xExclusive=TRUE! If a file still is opened, it can be deleted or renamed at the same time! Additionally a file can be opened several times (for reading and writing).
|
|
|
Output
|
eError
|
ERROR
|
Local library error ID (0: no error; 5101: time out)
|
|
hFile
|
CAA.HANDLE
|
File handle
|
|