AddMultiplicatedVector (FUN)

FUNCTION AddMultiplicatedVector : BOOL

This function will multiply the input vector by a scalar and will add this product to the input vector :

InOut:

Scope

Name

Type

Comment

Return

AddMultiplicatedVector

BOOL

The return value is not used.

Input

pv1

POINTER TO Vector3d

Pointer to input vector

pv2

POINTER TO Vector3d

Pointer to input vector

lrFactor

LREAL

Scalar multiplier

pv

POINTER TO Vector3D

Pointer to result