FUNCTION ReverseBitsInWORD : WORD
Function returns the WORD “wInput” with a reversed bit-order.
Example:
wInput = 16#0102 = 2#00000001 00000010 -> MEM.ReverseBitsInWORD(wInput) = 16#4080 = 2#01000000 10000000
Scope
Name
Type
Comment
Return
ReverseBitsInWORD
WORD
function returns a WORD with reversed bit-order of “wInput”
Input
wInput
WORD to reverse