CODESYS provides two different Ethernet/IP Scanners.
(1): A device that you insert directly below each network adapter An Ethernet/IP Scanner (IEC) can also be an adapter at the same time – functionally an originator and an adapter in one.
(2): A device that needs a special cifX adapter
You insert one or more EtherNet/IP adapters below a scanner.