Function: Opens the referenced visualization
Call: Visualization menu, context menu
Requirement: A frame element is selected.
If others are referenced in a visualization, then you can open them. In the element list (or in the Visualization Editor), select the referencing Frame or Tabs element. Then this command is available. The existing references are displayed in the following submenu. Click on the desired visualization and it will be opened.