Set_Attribute_List (FB)

FUNCTION_BLOCK Set_Attribute_List EXTENDS BaseService

This function blocks is used for setting the contents of selected attributes of the specified CIP Object class or instance.

Note

Data received and send needs to be swapped. See parent folder.

PROGRAM PLC_PRG
VAR
    arData            : ARRAY[0..9] OF BYTE;
    setAttributeList : ENIP.Set_Attribute_List ;
    arResponse      : ARRAY [0..9] OF BYTE;
END_VAR

setAttributeList(
    xExecute:= ,
    itfEtherNetIPDevice:= EtherNetIP_Adapter,    (* instance of the device (instance is found in the I/O Mapping of the device) *)
    eClass:= ENIP.CIPClass.TCPIPInterfaceObject, (* cip class which contains the desired attribute *)
    dwInstance:= 1,                              (* value of 0 is class level, range from 1..x is instance level *)
    pRequestData := ADR(arData);                    (* data buffer *)
       udiRequestDataSize := SIZEOF(arData);        (* size of the data buffer *)
       pResponseData := ADR(arResponse);            (* data buffer from the response *)
       udiResponseDataSize := SIZEOF(arResponse);   (* size of the data buffer from the response *)
    xDone=> ,
    xBusy=> ,
    xError=> ,
    eError=> );
    ;
InOut:

Scope

Name

Type

Comment

Inherited from

Input

xExecute

BOOL

Rising edge: Action starts

Falling edge: Resets outputs

If a falling edge occurs before the function block has completed its action, the outputs operate in the usual manner and are only reset if either the action is completed or in the event of an error. In this case, the corresponding output values (xDone, xError) are present at the outputs for exactly one cycle.

ETrig

Output

xDone

BOOL

TRUE: Action successfully completed

ETrig

xBusy

BOOL

TRUE: Function block active

ETrig

xError

BOOL

TRUE: Error occurred, function block aborts action

FALSE: No error

ETrig

Input

itfEtherNetIPDevice

IEtherNetIPService

BaseService

eClass

CIPClass

BaseService

dwInstance

DWORD

BaseService

Output

eError

ERROR

BaseService

Input

pRequestData

POINTER TO BYTE

udiRequestDataSize

UDINT

pResponseData

POINTER TO BYTE

udiResponseDataSize

UDINT