ControllerConfigUtil.GetDeviceInfo (METH)

METHOD GetDeviceInfo : BOOL

Get the detailed Profinet DeviceInfo data from a Profinet Slave node that is attached below a controller node.

InOut:

Scope

Name

Type

Comment

Return

GetDeviceInfo

BOOL

Input

pnDevice

DED.IDevice

The Profinet Slave device

Output

device

ProfinetCommon.DeviceInfo

The data of the current device. (Valid if return value is TRUE)