FUNCTION_BLOCK SMC_RecomputeABCSlopes
Recomputes the slopes of the additional axes A,B,C so that a smooth movement results. The slope at the end of elemnt i is set as (AddAxisValue(i+1) - AddAxisValue(i-1)) / (ElementLength(i) + ElementLength(i+1)). At a stop, the slope is either set to zero, or set so that the interpolation of the additional axis is linear, depending on the input modeAtStop.
InOut:
|
Scope
|
Name
|
Type
|
Initial
|
Comment
|
Input
|
bExecute
|
BOOL
|
|
Starts on the rising edge
|
poqDataIn
|
POINTER TO SMC_OUTQUEUE
|
|
Input path queue
|
nSizeOutQueue
|
UDINT
|
|
The size of pbyBufferOutQueue in bytes
|
pbyBufferOutQueue
|
POINTER TO ARRAY [0..0] OF SMC_GEOINFO
|
|
The buffer for the output queue
|
dAngleTol
|
LREAL
|
0.001
|
The angle tolerence (in angular degrees) to detect stops between elements
|
modeNoStop
|
SMC_ABC_SLOPES_NO_STOP
|
|
Determines how the slope is set at element transitions without a stop. The default is SET_SMOOTH_CARDINAL.
|
modeAtStop
|
SMC_ABC_SLOPES_AT_STOP
|
|
Determines how the slope is set at element transitions with a stop. The default, due to compatibility with older versions, is SET_ZERO.
|
Output
|
bDone
|
BOOL
|
|
Indicates the entire input path has been processed
|
bBusy
|
BOOL
|
|
Indicates the function block is still busy processing
|
bError
|
BOOL
|
|
An error has occurred
|
wErrorID
|
SMC_ERROR
|
|
Error-ID
|
poqDataOut
|
POINTER TO SMC_OUTQUEUE
|
|
The queue for the output path
|
|
Structure: