SMC_TRAFOF_Bipod_Arm (FB)

FUNCTION_BLOCK SMC_TRAFOF_Bipod_Arm

The transformation computes the forward transformation of a bipod with two rotary axes. See SMC_TRAFO_Bipod_Arm for a description.

Note

For more information on the supported transformations, see the chapter on CNC transformations.

InOut:

Scope

Name

Type

Initial

Comment

Input

dArmLength1

LREAL

Length of Arm1 connected to motor

dArmLength2

LREAL

Length of Arm2 from Arm1 to linked connection

dDistance

LREAL

Distance of the two motors

dOffsetA

LREAL

0

Additional offset of axis A in SoftMotion units

dOffsetB

LREAL

0

Additional offset of axis B in SoftMotion units

Output

bError

BOOL

TRUE, if position is invalid

dx

LREAL

X-position of manipulator

dy

LREAL

Y-position of manipulator

Inout

DriveA

AXIS_REF_SM3

Reference to axis A

DriveB

AXIS_REF_SM3

Reference to axis B