SR_<Camera Name> - Logic (Method)

Overview

Type:

Method

Available as of:

V2.3.1.0

Functional Description

The method Logic is automatically called cyclically and can be used to program the logic for the camera.

The method has no inputs/outputs.