FUNCTION_BLOCK DynamicTraceLoaderRemote EXTENDS DynamicTraceLoader
This function block is an enhancement of the DynamicTraceLoader function block to load a trace configuration from the local application and to create the packet on the remote PLC.
Properties:
Methods:
Initialize, inherited from DynamicTraceLoader
Structure: