Return
|
Resolve
|
BOOL
|
|
Input
|
psApplication
|
POINTER TO STRING
|
Points to a string containing the name of the application
|
pszVariable
|
POINTER TO STRING
|
Points to the name of the trace variable, that has to be resolved
|
pTraceVariableAddress
|
POINTER TO TraceVariableAddress
|
Points to a TraceVariableAddress variable, where the address definition of the variable will be stored.
|
pulSize
|
POINTER TO UDINT
|
Points to an UDINT variable, where the size of the variable will be be stored
|
pClass
|
POINTER TO TypeClass3
|
Type class of the variable. See enum IBase.TypeClass for the possible values.
|