FUNCTION IsValidRune : BOOL
Reports whether diRune can be legally encoded as UTF-8.
Code points that are out of range or a surrogate half are illegal.
Scope
Name
Type
Return
IsValidRune
BOOL
Input
diRune
RUNE