VisuFbAnalyzeTextVarsDateTimeOnly.GetAsLINT (METH)

METHOD GetAsLINT : LINT

Takes the current variable value and converts it into a LINT value. This method can be only used if the variable’s type is TIME, TOD or LTIME.

InOut:

Scope

Name

Type

Return

GetAsLINT

LINT